How to avoid CAN bootloader call the _COPY function.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to avoid CAN bootloader call the _COPY function.

ソリューションへジャンプ
4,193件の閲覧回数
xyfan
Contributor I

Hi,

I am working with a MC9S12XEP100 CAN bootloader project. After compiled the project I found the bootloader used two function, _COPY and _CASE_CHECKED_BYTE.  These two functions are generated from rtshc12.c.o (ansixbi.lib). Because my bootloader uses these two functions. I can't erase the NON_BANKED segment, where these two functions located. Or my bootloader will die. That means I can't update the NON_BANKED segment.

I want to ask is there any way to avoid my bootloader using these two functions. In order to let me update NON_BANKED segment as well as user application.

Thanks.

Here's some segment of my project.

void CanStatusAck(UINT8 sta)
{
TxMsg.ID = UpLoadID;
TxMsg.DtLen = 1;
TxData[0] = sta;
TxMsg.data=(UINT8 *)&TxData[0];

/*It looks like the _COPY function is called there*/
(void)CanTxFrame(TxMsg);
}

UINT8 CanTxFrame(CanMsg_t msg)
{
unsigned char send_buf, sp;
if(msg.DtLen > 8)
return(FALSE);

if(CAN0CTL0_SYNCH==0)
return(FALSE);

send_buf = 0;

do
{
CAN0TBSEL=CAN0TFLG;
send_buf=CAN0TBSEL;
}
while(!send_buf);
CAN0TXIDR0 = (unsigned char)(msg.ID>>3);
CAN0TXIDR1 = (unsigned char)(msg.ID<<5);

for(sp = 0; sp < msg.DtLen; sp++)
*((&CAN0TXDSR0)+sp) = msg.data[sp];

CAN0TXDLR = msg.DtLen;

CAN0TFLG = send_buf;

return(TRUE);
}

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
4,016件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi XY,

Thank you for testing and results.

 

The “case” command might be replaced by set of “if” conditions.

 

How did you move bootloader code from flash to RAM?

The first principle is defining code directly at RAM by #pragma CODE_SEG linker commands. The code is automatically loaded into RAM during startup.

The second principle is creating code on Flash and move it into RAM by some copy function. Te example might be for example AN4258 software.

 

The compiler might be configured for generating position-independent code by -Pic compiler option. However I suppose, that it will not solve this issue.

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

6 返答(返信)
4,016件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi XY,

Unfortunately, I was not able replicate it on my side yet. I guess, that different compiler settings might be a reason.

 

  1. For testing purpose, you may try to add asm NOP; commands into your code. For example:

for(sp = 0; sp < msg.DtLen; sp++)

{

*((&CAN0TXDSR0)+sp) = msg.data[sp];

asm NOP;

}

The assembler code blocks compiler optimizations.

 

  1. Please try also change optimization from size to time (-Os, -Ot).

 

  1. You may also try to add -Oilib: Optimize Library Functions compiler option. This enables the compiler to optimize specific known library functions by inlining.

 

  1. Please check whether your Compiler settings refers to the selected ANSI library. See "c:\Program Files (x86)\Freescale\CWS12v5.2\lib\hc12c\readme.txt"

 

  1. In extreme case, you may copy assembler code from rtshc12.c file directly into your C function.

 

If nothing helps, please send us your project for review. If it is not public, you may create a ticket for us:

https://community.nxp.com/docs/DOC-329745

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
4,016件の閲覧回数
xyfan
Contributor I

Hi

I have tried all the possible solutions you wrote, but none of them works. I think it's when a big struck to be sent into another function as a parameter that the project call the _COPY. In the code I posted earlier. When the TxMsg (it's a struct like snipaste20170615_012745.jpg) being sent into CanTxFrame(TxMsg) as a parameter, the _COPY was called (by compiler). In order to remove the parameter transfer process. I put the  CanTxFrame's code directly in CanStatusAck function and it works. The _COPY function was removed from my bootloader successfully. 

But there is also another named _CASE_CHECKED_BYTE being called when I use "case". I can't find solutions to remove _CASE_CHECKED_BYTE yet.

Thank you anyway.

0 件の賞賛
返信
4,017件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi XY,

Thank you for testing and results.

 

The “case” command might be replaced by set of “if” conditions.

 

How did you move bootloader code from flash to RAM?

The first principle is defining code directly at RAM by #pragma CODE_SEG linker commands. The code is automatically loaded into RAM during startup.

The second principle is creating code on Flash and move it into RAM by some copy function. Te example might be for example AN4258 software.

 

The compiler might be configured for generating position-independent code by -Pic compiler option. However I suppose, that it will not solve this issue.

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,016件の閲覧回数
xyfan
Contributor I

Hi

My bootloader code was written on the flash and moved to ram by a copy function. I removed _COPY function yesterday. I changed "case" command into "if else" condition just now and the _CASE_CHECKED_BYTE was removed successfully! So these two functions will not be called anymore. I can put the NON_BANKED segment into ROM_C000 finally.  I think the NON_BANKED can be updated by bootloader too.

Thank you for your help.

0 件の賞賛
返信
4,016件の閲覧回数
RadekS
NXP Employee
NXP Employee

You are welcome.

I am glad that it works now.

Have a great day,
Radek

0 件の賞賛
返信
4,016件の閲覧回数
407214944
Contributor I

Now I am ready to use the can_bootloader to upload program ,And where to download the project of can_bootloader .Can you send the project ,Involved in the data to me? My email is [email protected].3ks!

0 件の賞賛
返信