S12 can bootloader ask for help!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12 can bootloader ask for help!

2,155 Views
407214944
Contributor I

On a recent project with MS12G128 this MCU, through CAN do IAP, namely the Bootloader.Can you provide this information?Whether there is the 16-bit machine series Can_bootloader engineering?Thank you.

Tags (3)
0 Kudos
Reply
1 Reply

1,805 Views
RadekS
NXP Employee
NXP Employee

Hi 义福 郭,

Unfortunately, I am not aware of any official CAN bootloader directly for S12G.

 

I can recommend our application note AN4258 Serial Bootloader for S12(X) Microcontrollers Based on 180 nm Technology

http://www.nxp.com/files/microcontrollers/doc/app_note/AN4258.pdf

http://www.nxp.com/files/microcontrollers/doc/app_note/AN4258SW.zip

You can use it as base for your own bootloader and just add CAN interface. The AN4258 directly implements only SCI channel.

 

You may use also AN3391 LFAE Bootloader Example and Interface for use with AN2546 (CAN bootloader for S12XE)

http://www.nxp.com/files/microcontrollers/doc/app_note/AN3391.pdf

http://www.nxp.com/files/microcontrollers/doc/app_note/AN3391SW.zip

for your inspiration.

 

The pack of simple CAN examples is attached.

Optionally you may use directly CAN driver:

http://www.nxp.com/files/microcontrollers/software/device_drivers/MSCAN_S12_DEVD.zip

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------