ECT Function of priority?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ECT Function of priority?

ソリューションへジャンプ
2,233件の閲覧回数
Kr_Blue
Contributor I

Hi.

 

Enhanced Capture Timer (ECT) function of the IOS 0 ~ 7 channels with the highest priority?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,680件の閲覧回数
kef
Specialist I

Do you mean which ECT channel has highest interrupt priority? By default higher interrupt priority have interrupts with higher interrupt vector address. Among ECT channels, channel 0 has highest vector address and highest interrupt priority. On S12 you can specify highest priority interrupt using HPRIO register. On S12X you can adjust interrupt priority levels for all interrupts using INT_CFADDR and INT_CFDATAn registers.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,681件の閲覧回数
kef
Specialist I

Do you mean which ECT channel has highest interrupt priority? By default higher interrupt priority have interrupts with higher interrupt vector address. Among ECT channels, channel 0 has highest vector address and highest interrupt priority. On S12 you can specify highest priority interrupt using HPRIO register. On S12X you can adjust interrupt priority levels for all interrupts using INT_CFADDR and INT_CFDATAn registers.

0 件の賞賛
返信
1,680件の閲覧回数
Kr_Blue
Contributor I

Thank you for you'r answer.

0 件の賞賛
返信