ECT Function of priority?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ECT Function of priority?

Jump to solution
2,239 Views
Kr_Blue
Contributor I

Hi.

 

Enhanced Capture Timer (ECT) function of the IOS 0 ~ 7 channels with the highest priority?

Labels (1)
0 Kudos
Reply
1 Solution
1,686 Views
kef
Specialist I

Do you mean which ECT channel has highest interrupt priority? By default higher interrupt priority have interrupts with higher interrupt vector address. Among ECT channels, channel 0 has highest vector address and highest interrupt priority. On S12 you can specify highest priority interrupt using HPRIO register. On S12X you can adjust interrupt priority levels for all interrupts using INT_CFADDR and INT_CFDATAn registers.

View solution in original post

0 Kudos
Reply
2 Replies
1,687 Views
kef
Specialist I

Do you mean which ECT channel has highest interrupt priority? By default higher interrupt priority have interrupts with higher interrupt vector address. Among ECT channels, channel 0 has highest vector address and highest interrupt priority. On S12 you can specify highest priority interrupt using HPRIO register. On S12X you can adjust interrupt priority levels for all interrupts using INT_CFADDR and INT_CFDATAn registers.

0 Kudos
Reply
1,686 Views
Kr_Blue
Contributor I

Thank you for you'r answer.

0 Kudos
Reply