DEVKIT-S12XE Use usb as serial port

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DEVKIT-S12XE Use usb as serial port

Jump to solution
1,713 Views
Usuari
Contributor I

DEVKIT-S12XE includes an On board OSBDM/Serial bridge to program and debbug. It uses a MC9S08JM60CGTE connected to S12XEP100 UART2 port (PJ0;PJ1 pins) for this purpose.

Question: Is it possible to bridge UART2 to USB?

That is: use the UART2 to send/receive serial through USB connector

0 Kudos
Reply
1 Solution
1,684 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @Usuari,

Yes, it is possible to use the USB emulated UART (SCI2), it works by default.

 

Regards,

Daniel

 

 

 

View solution in original post

1 Reply
1,685 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @Usuari,

Yes, it is possible to use the USB emulated UART (SCI2), it works by default.

 

Regards,

Daniel