DEVKIT-S12XE Use usb as serial port

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

DEVKIT-S12XE Use usb as serial port

跳至解决方案
1,695 次查看
Usuari
Contributor I

DEVKIT-S12XE includes an On board OSBDM/Serial bridge to program and debbug. It uses a MC9S08JM60CGTE connected to S12XEP100 UART2 port (PJ0;PJ1 pins) for this purpose.

Question: Is it possible to bridge UART2 to USB?

That is: use the UART2 to send/receive serial through USB connector

标记 (4)
0 项奖励
回复
1 解答
1,666 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @Usuari,

Yes, it is possible to use the USB emulated UART (SCI2), it works by default.

 

Regards,

Daniel

 

 

 

在原帖中查看解决方案

1 回复
1,667 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @Usuari,

Yes, it is possible to use the USB emulated UART (SCI2), it works by default.

 

Regards,

Daniel