DEVKIT-S12XE Use usb as serial port

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DEVKIT-S12XE Use usb as serial port

ソリューションへジャンプ
1,697件の閲覧回数
Usuari
Contributor I

DEVKIT-S12XE includes an On board OSBDM/Serial bridge to program and debbug. It uses a MC9S08JM60CGTE connected to S12XEP100 UART2 port (PJ0;PJ1 pins) for this purpose.

Question: Is it possible to bridge UART2 to USB?

That is: use the UART2 to send/receive serial through USB connector

タグ(4)
0 件の賞賛
返信
1 解決策
1,668件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @Usuari,

Yes, it is possible to use the USB emulated UART (SCI2), it works by default.

 

Regards,

Daniel

 

 

 

元の投稿で解決策を見る

1 返信
1,669件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @Usuari,

Yes, it is possible to use the USB emulated UART (SCI2), it works by default.

 

Regards,

Daniel