CW communication with 9S12XDP512

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW communication with 9S12XDP512

Jump to solution
1,716 Views
roberthiebert
Senior Contributor I

I have just installed a Special Edition of CW, IDE V5.9.0 build 5294. I would like to use the AD9S12XDP512M2 development board from Technological Arts and use CW to program in assembler. I am not clear on what additional hardware I will require to communicate with the board and load the .s19 file.

Do I have any options here?

Labels (1)
0 Kudos
Reply
1 Solution
1,542 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

P&E also has some other pod can support HCS12(X). you can see details in the related webpage:

Cyclone PRO

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=1

USB Multilink Universal

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320137

USB Multilink Universal FX

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320143

they are more expensive than P&E BDM multilink.  P&E BDM multilink is most popular used emulator for HCS12(x) family.

------------------------------------------------

this answer is for you. if it answers your question, please click on the "correct answer" button.

Best Regards,

JunZhang

View solution in original post

0 Kudos
Reply
6 Replies
1,542 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hi Robert,

the recommend program pod for this board is P&E BDM multilink. see this link: http://www.pemicro.com/products/product_viewDetails.cfm?product_id=33


if you have any question on this, please contact again.



------------------------------------------------

this answer is for you. if it answers your question, please click on the "correct answer" button.

Best Regards,

JunZhang

0 Kudos
Reply
1,542 Views
roberthiebert
Senior Contributor I

Do I have to purchase any software to use the P&E BDM multilink?

0 Kudos
Reply
1,542 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

No, no software needed to use P&E BDM Multilink.

------------------------------------------------

this answer is for you. if it answers your question, please click on the "correct answer" button.

Best Regards,

JunZhang

0 Kudos
Reply
1,542 Views
roberthiebert
Senior Contributor I

That's good news. Do I have any options other than the P&E BDM multilink?

0 Kudos
Reply
1,543 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

P&E also has some other pod can support HCS12(X). you can see details in the related webpage:

Cyclone PRO

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=1

USB Multilink Universal

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320137

USB Multilink Universal FX

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320143

they are more expensive than P&E BDM multilink.  P&E BDM multilink is most popular used emulator for HCS12(x) family.

------------------------------------------------

this answer is for you. if it answers your question, please click on the "correct answer" button.

Best Regards,

JunZhang

0 Kudos
Reply
1,542 Views
roberthiebert
Senior Contributor I

Thanks again

0 Kudos
Reply