9S12X assembly instruction clarification

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

9S12X assembly instruction clarification

ソリューションへジャンプ
2,573件の閲覧回数
roberthiebert
Senior Contributor I

I have some assembly code written for the 9S12X that I am trying to figure out what it does. One instruction is:

ADDD 8,SP   I believe that is and instruction to add the contents of Accu D with the contents at stack +8.

Another instruction is :

ADDD (8+2),SP  Is that the same as ADDD 10,SP which would be an instruction to add the contents of Accu D with the contents at stack +10?

Regards,

Robert

0 件の賞賛
返信
1 解決策
2,518件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Robert,

danielmartynek_0-1626351242178.png

danielmartynek_1-1626351293290.png

So, (8+2) is an offset to location M which is the SP in this case

danielmartynek_2-1626351360222.png

danielmartynek_3-1626351397508.png

M = 0x6E, M+1 = 0x88 which is added to D (A = 0x00, B=0x00).

D = 0x6E88

 

Regards,

Daniel

 

 

 

 

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,535件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Robert,

I'm sorry for the delay.

It is explained in the CPU12X reference manual v01.04.

danielmartynek_0-1626178642806.png

It concatenates the content of M with the content of M+1 and adds it to the accumulator D.

I believe you can test it in CW 5.2, there is a simulator if you don't have any board.

 

Regards,

Daniel

 

 

0 件の賞賛
返信
2,529件の閲覧回数
roberthiebert
Senior Contributor I

Hi Daniel,

Thanks for your response. Yes, I had looked up the ADDD instruction as you posted, and it makes sense when ADDD is followed by a memory location, but I am still confused as to what (8+2),SP means. I'm afraid that any manipulations on the stack confuse me easily.

Regards,

Robert

0 件の賞賛
返信
2,511件の閲覧回数
roberthiebert
Senior Contributor I

Hi Daniel,

Got it, and thanks so much for the lesson in debugging. So it looks like I was correct in my original post where I thought that (8+2),SP could be the same as 10,SP. I wonder why the author would chose to do it that way?

Regards,

Robert

0 件の賞賛
返信
2,519件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Robert,

danielmartynek_0-1626351242178.png

danielmartynek_1-1626351293290.png

So, (8+2) is an offset to location M which is the SP in this case

danielmartynek_2-1626351360222.png

danielmartynek_3-1626351397508.png

M = 0x6E, M+1 = 0x88 which is added to D (A = 0x00, B=0x00).

D = 0x6E88

 

Regards,

Daniel

 

 

 

 

 

 

0 件の賞賛
返信