9S12X assembly instruction clarification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

9S12X assembly instruction clarification

Jump to solution
3,479 Views
roberthiebert
Senior Contributor I

I have some assembly code written for the 9S12X that I am trying to figure out what it does. One instruction is:

ADDD 8,SP   I believe that is and instruction to add the contents of Accu D with the contents at stack +8.

Another instruction is :

ADDD (8+2),SP  Is that the same as ADDD 10,SP which would be an instruction to add the contents of Accu D with the contents at stack +10?

Regards,

Robert

0 Kudos
Reply
1 Solution
3,424 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Robert,

danielmartynek_0-1626351242178.png

danielmartynek_1-1626351293290.png

So, (8+2) is an offset to location M which is the SP in this case

danielmartynek_2-1626351360222.png

danielmartynek_3-1626351397508.png

M = 0x6E, M+1 = 0x88 which is added to D (A = 0x00, B=0x00).

D = 0x6E88

 

Regards,

Daniel

 

 

 

 

 

 

View solution in original post

0 Kudos
Reply
4 Replies
3,441 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Robert,

I'm sorry for the delay.

It is explained in the CPU12X reference manual v01.04.

danielmartynek_0-1626178642806.png

It concatenates the content of M with the content of M+1 and adds it to the accumulator D.

I believe you can test it in CW 5.2, there is a simulator if you don't have any board.

 

Regards,

Daniel

 

 

0 Kudos
Reply
3,435 Views
roberthiebert
Senior Contributor I

Hi Daniel,

Thanks for your response. Yes, I had looked up the ADDD instruction as you posted, and it makes sense when ADDD is followed by a memory location, but I am still confused as to what (8+2),SP means. I'm afraid that any manipulations on the stack confuse me easily.

Regards,

Robert

0 Kudos
Reply
3,417 Views
roberthiebert
Senior Contributor I

Hi Daniel,

Got it, and thanks so much for the lesson in debugging. So it looks like I was correct in my original post where I thought that (8+2),SP could be the same as 10,SP. I wonder why the author would chose to do it that way?

Regards,

Robert

0 Kudos
Reply
3,425 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Robert,

danielmartynek_0-1626351242178.png

danielmartynek_1-1626351293290.png

So, (8+2) is an offset to location M which is the SP in this case

danielmartynek_2-1626351360222.png

danielmartynek_3-1626351397508.png

M = 0x6E, M+1 = 0x88 which is added to D (A = 0x00, B=0x00).

D = 0x6E88

 

Regards,

Daniel

 

 

 

 

 

 

0 Kudos
Reply