No operation or BLE connection (Datecode 1827)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

No operation or BLE connection (Datecode 1827)

4,022件の閲覧回数
marioarh
Contributor I

I tried 5 boards (DC1827) and all of them a hanging up when I turn them on at the screen "Powered by Atmosphere" If i can run one, then I am not able to connect to the BLE. I can't find the device. Do you know the bug?

0 件の賞賛
返信
4 返答(返信)

3,813件の閲覧回数
Eric_Ma
NXP Employee
NXP Employee

HI Mario,

On top of Richard's question:

- Do you confirm the top right blue and white leds are fixed on ?

If yes, please try the fix proposed in this post:

https://community.nxp.com/thread/481369

0 件の賞賛
返信

3,813件の閲覧回数
marioarh
Contributor I

Hi Eric, this was a helpful hint, but from time to time it freezes again.

I also found out, when i try to establish the BLE connection (i find the device now) within the NXP Rapid IoT App, the device reboots but the connection is not established. Is this a known bug?

Thanks Mario

0 件の賞賛
返信

3,813件の閲覧回数
richard_laborde
Contributor III

marioarh‌ - Is this out of the box, or after programming with a project? Have you reviewed the Serial Console output? That and the .atmo file would help diagnose the issue. Thanks

0 件の賞賛
返信

3,813件の閲覧回数
marioarh
Contributor I

Hi Richard, it is out of the box. So I am not able to do anything. When I am resetting the kit, from time to time it runs up, but after a reboot it already crashes.  The other thing is, that I installed the NXP weather station, and i can't find any BLE devices with the app.

0 件の賞賛
返信