Azure IoT Middleware support in k8x series

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Azure IoT Middleware support in k8x series

1,447件の閲覧回数
pritesh_shah
Contributor I

Hi,

We are developing an application using kinetis controller which required features of an azure IoT.

while selecting an azure IoT middleware component in "MCUxpresso software development kit", it is not showing the k8x series controllers in the whitelist.

So Need to confirm that Azure IoT is supported or not in k8x series.

タグ(2)
0 件の賞賛
返信
1 返信

1,338件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello,

According to Azure IoT documentation on their website it can be used with the microcontroller. You were not able to find it in the SDK builder, because there has not been an implementation or development of examples utlizing this specific microcontroller from our teams. The implementation and usage in custom applications will have to be developed by the customer.

Best Regards,

Sabina