Azure IoT Middleware support in k8x series

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Azure IoT Middleware support in k8x series

1,448 Views
pritesh_shah
Contributor I

Hi,

We are developing an application using kinetis controller which required features of an azure IoT.

while selecting an azure IoT middleware component in "MCUxpresso software development kit", it is not showing the k8x series controllers in the whitelist.

So Need to confirm that Azure IoT is supported or not in k8x series.

Tags (2)
0 Kudos
Reply
1 Reply

1,339 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello,

According to Azure IoT documentation on their website it can be used with the microcontroller. You were not able to find it in the SDK builder, because there has not been an implementation or development of examples utlizing this specific microcontroller from our teams. The implementation and usage in custom applications will have to be developed by the customer.

Best Regards,

Sabina