is dpaa2-qdma driver compatible with LS1046a

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

is dpaa2-qdma driver compatible with LS1046a

1,391件の閲覧回数
basudebdas
Contributor I

Hi,

Does any one know if the dpaa2-qdma driver is compatible with LS1046a processor ?

0 件の賞賛
返信
1 返信

1,297件の閲覧回数
Pavel
NXP Employee
NXP Employee

The LS1046a supports DPAA1. LSDK 18.12 documentation contains information that "QDMA can support Layerscape platform with DPAA1 or DPAA2." See the Section 7.2.10 of LSDK 18.12 documentation.

Also this documentation shows .dts example for the LS1046a.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信