is dpaa2-qdma driver compatible with LS1046a

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

is dpaa2-qdma driver compatible with LS1046a

1,393 Views
basudebdas
Contributor I

Hi,

Does any one know if the dpaa2-qdma driver is compatible with LS1046a processor ?

0 Kudos
Reply
1 Reply

1,299 Views
Pavel
NXP Employee
NXP Employee

The LS1046a supports DPAA1. LSDK 18.12 documentation contains information that "QDMA can support Layerscape platform with DPAA1 or DPAA2." See the Section 7.2.10 of LSDK 18.12 documentation.

Also this documentation shows .dts example for the LS1046a.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply