execute binary compiled at LS1021A to run on LS1046A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

execute binary compiled at LS1021A to run on LS1046A

1,095 Views
ihaymov
Contributor II

I am trying to figure out if I can develop at TWR-LS1021 instead of other EVB  based on LS1046 using 32 bit compiler and to be able to run the executable binary at the LS1046 ?

I will need to test, PCIe (gen. 2 or 3), USB driver, IFC driver, GPIO.

What are the choices (cross-compile / use different yocto's for each platform)?

Tags (2)
0 Kudos
Reply
1 Reply

1,001 Views
alexander_yakov
NXP Employee
NXP Employee

We do not have an experience in using LS1021A-based board for development a software, intended to be executed at LS1046A board. We recommend using LS1046A-based development board for this purpose.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------