Is it possible to run memac10 in independent mode on the t2081 processor? A board is configuring memac10 to use the second RGMII interface. Memac3 is using the first RGMII interface and works fine in independent mode. However memac10 is 1 / 2.5 / 10Gbps, so I'm wondering if it can not be used in independent mode.
Thanks!
Mark
The T2081 mEMAC10 can operate in independent mode.