e6500 special registers not visible when debugging with apptrk

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

e6500 special registers not visible when debugging with apptrk

跳至解决方案
1,430 次查看
aloishahn
Contributor III

Hi,

this is a question regarding CW 10.4 PA debugging using the apptrk debug server on the target side, actually a t2080rdb.

When I run a CW PA debug session, with apptrk as debug server, the register view is missing special e6500 registers.

In contrast, in a debug session via jtag (CodeWarrior TAP), the Debug Perspective shows all the special registers like regPPC Altivec, e6500 Special Registers, etc.

(see attached screenshots)

Should apptrk show the special e6500 registers ?

best regards

Alois

special registers missing with apptrk connection

Special-Registers-missing-Linux-apptrk.png

special registers shown with bareborad CodeWarrior TAP JTAG connection

Special-Registers-BareBoard-CW-TAP.png

0 项奖励
回复
1 解答
1,302 次查看
catalindemergia
Contributor IV

Hi,

This is true, you cannot see all of the registers with apptrk as you would see with a bareboard application.

This is a limitation of the current implementation.

regards,

Catalin

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,303 次查看
catalindemergia
Contributor IV

Hi,

This is true, you cannot see all of the registers with apptrk as you would see with a bareboard application.

This is a limitation of the current implementation.

regards,

Catalin

0 项奖励
回复