e6500 special registers not visible when debugging with apptrk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

e6500 special registers not visible when debugging with apptrk

Jump to solution
1,433 Views
aloishahn
Contributor III

Hi,

this is a question regarding CW 10.4 PA debugging using the apptrk debug server on the target side, actually a t2080rdb.

When I run a CW PA debug session, with apptrk as debug server, the register view is missing special e6500 registers.

In contrast, in a debug session via jtag (CodeWarrior TAP), the Debug Perspective shows all the special registers like regPPC Altivec, e6500 Special Registers, etc.

(see attached screenshots)

Should apptrk show the special e6500 registers ?

best regards

Alois

special registers missing with apptrk connection

Special-Registers-missing-Linux-apptrk.png

special registers shown with bareborad CodeWarrior TAP JTAG connection

Special-Registers-BareBoard-CW-TAP.png

0 Kudos
Reply
1 Solution
1,305 Views
catalindemergia
Contributor IV

Hi,

This is true, you cannot see all of the registers with apptrk as you would see with a bareboard application.

This is a limitation of the current implementation.

regards,

Catalin

View solution in original post

0 Kudos
Reply
1 Reply
1,306 Views
catalindemergia
Contributor IV

Hi,

This is true, you cannot see all of the registers with apptrk as you would see with a bareboard application.

This is a limitation of the current implementation.

regards,

Catalin

0 Kudos
Reply