T1042 Output pin IBIS Model

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

T1042 Output pin IBIS Model

跳至解决方案
3,677 次查看
qammarabbas
Contributor IV

Hi,

I am simulating T1042's Serdes interface in Hyperlynx. The IBIS model of T1042 does not allow me to set the transmitter pins (AD17 and AE17) as output. Moreover, these pins are mentioned as output in the datasheet as well. Kindly let me know what can i do to configure these differential pins as output in Hyperlynx?

标记 (1)
1 解答
3,532 次查看
ufedor
NXP Employee
NXP Employee

It is required to use IBIS-AMI model in this case.

在原帖中查看解决方案

0 项奖励
回复
5 回复数
3,533 次查看
ufedor
NXP Employee
NXP Employee

It is required to use IBIS-AMI model in this case.

0 项奖励
回复
3,532 次查看
qammarabbas
Contributor IV

Thanks ufedor‌. I have created a case for it. Please let me know if AMI model is also required for the receiver?

0 项奖励
回复
3,532 次查看
ufedor
NXP Employee
NXP Employee

The IBIS-AMI model contains TX and RX models.

0 项奖励
回复
3,532 次查看
qammarabbas
Contributor IV

What i could understand from this statement is that the IBIS-AMI model of T1042 will be having IBIS-AMI model of the receiver (FPGA in my case) as well. Is it right?

0 项奖励
回复
3,532 次查看
ufedor
NXP Employee
NXP Employee

> the IBIS-AMI model of T1042 will be having IBIS-AMI model of the receiver (FPGA in my case) as well.

Of course - not.

The T1042 IBIS-AMI package contains TX and RX models of the T1042.