T1040RDB schematic diagram QUESTION

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1040RDB schematic diagram QUESTION

Jump to solution
1,460 Views
于立冬
Contributor I

IN IFC page  have "interposer por cfg" it is no introdue on T1040 reference manual,the pin also call "cfg_rcw_src*" and all pin have res to pull or down,like r809 r810 (cfg_dram_type cfg_elbc_ecc)and so on  can delete?those pin not define in manual, I must reserve the design?

0 Kudos
Reply
1 Solution
1,347 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

The "interposer por cfg" is not related to any T1040 signal, you can ignore this name given by board designer for signal group. The “cfg_rcw_src*" are mistypes. You can see f.e. that the “cfg_rcw_src2” becomes cfg _eng_use1 (it is correct name) on page 26. The “cfg_elbc_ecc” is obsolete, it does not require for external termination during power-on reset configuration. The”cfg_dram_type” is valid name and described in the reference manual. There is T1040 Family Design Checklist on the nxp site. It is convenient way to check signal termination in this document. If you still doubt then check signal in Table 1. Pinout list by bus of the QorIQ T1040, T1020 Data Sheet.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,348 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

The "interposer por cfg" is not related to any T1040 signal, you can ignore this name given by board designer for signal group. The “cfg_rcw_src*" are mistypes. You can see f.e. that the “cfg_rcw_src2” becomes cfg _eng_use1 (it is correct name) on page 26. The “cfg_elbc_ecc” is obsolete, it does not require for external termination during power-on reset configuration. The”cfg_dram_type” is valid name and described in the reference manual. There is T1040 Family Design Checklist on the nxp site. It is convenient way to check signal termination in this document. If you still doubt then check signal in Table 1. Pinout list by bus of the QorIQ T1040, T1020 Data Sheet.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply