T0142 MAC Level line loopback

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T0142 MAC Level line loopback

1,522 Views
pregache
Contributor II

Hello, in order to validate the SGMII links of out T1042 design (connected to FPGAs and GbE device) I am looking for a way to loopback the SMGII link on itself (from en external point of view), or better at the MAC level.

That is, incoming traffic received on the RX line of a SGMII is looped back onto the TX.

So far I have not been able to fin any related feature in teh T0140RM or other document.

Is this possible ? Where should I look at ?

Thank you

Pascal 

0 Kudos
Reply
1 Reply

1,462 Views
ufedor
NXP Employee
NXP Employee

Requested loopback functionality is not available.

0 Kudos
Reply