Sizeof Internal data memory(SRAM) for LS2084a

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sizeof Internal data memory(SRAM) for LS2084a

Jump to solution
1,112 Views
bmohan
Contributor IV

How to load a u-boot.elf or u-boot.bin using lauterbach JTAG in internal memory of LS2084a ?

Is LS2084a has any internal SRAM memory and what is memory location for internal SRAM memory and size of it ?

Currently U-BOOT text location started at 0x30100000. As per "include/configs/ls2080a_common.h", "CONFIG_SYS_TEXT_BASE" set to 0x30100000.

Tags (1)
0 Kudos
Reply
1 Solution
965 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Balaji Mohan,

Please refer to the following memory map for OCRAM(internal memory) from LS1024A Reference Manual, OCRAM is from 0x18000000 to 0x181fffff.

pastedImage_1.png

Please refer to the following memory map, the address 0x30100000 is IFC NOR flash.

pastedImage_2.png

You could refer to u-boot debugging section in https://community.nxp.com/docs/DOC-331981 .


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
966 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Balaji Mohan,

Please refer to the following memory map for OCRAM(internal memory) from LS1024A Reference Manual, OCRAM is from 0x18000000 to 0x181fffff.

pastedImage_1.png

Please refer to the following memory map, the address 0x30100000 is IFC NOR flash.

pastedImage_2.png

You could refer to u-boot debugging section in https://community.nxp.com/docs/DOC-331981 .


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------