Hi,
I was able to find the "Installation procedure of QorIQ-SDK-V1.6-SOURCE-20140619-yocto.iso (QorIQ linux SDK1.pdf)" as a document from Freescale community.
Is there any similar document available for installing sdk version 1.7? or is it okay to follow the same steps used for version 1.6?
Kindly confirm.
Thanks,
Agnes
Hi,
Thank you for your quick support.
As of now I am referring the same.
Thanks,
Agnes
Hello Agnes Amreetha,
In addition, you also need to run to "poky/scripts/host-prepare.sh" to install the required packages on your host machine, scripts have been moved into poky folder in SDK 1.7.
Thanks,
Yiping
Hello Agnes Amreetha,
You could follow the document QorIQ Linux SDK 1.6 Working With Yocto, please note when sets up a build environment, you need to use "source ./poky/fsl-setup-poky -m <platform>" rather than "source ./fsl-setup-poky -m <platform>".
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------