P3041 DMA Base address.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P3041 DMA Base address.

Jump to solution
1,872 Views
dshard
Contributor I

Hello!

Can u help me with P3041 DMA base adrress plese?

Tags (1)
0 Kudos
Reply
1 Solution
1,705 Views
Bulat
NXP Employee
NXP Employee

I am not sure what you mean, probably location of the DMA blocks in the internal memory map?

Offset of DMA1  is CCSRBAR + 0x10_0000;

offset of DMA2 is CCSRBAR + 0x10_1000;

Regards,

Bulat

View solution in original post

0 Kudos
Reply
1 Reply
1,706 Views
Bulat
NXP Employee
NXP Employee

I am not sure what you mean, probably location of the DMA blocks in the internal memory map?

Offset of DMA1  is CCSRBAR + 0x10_0000;

offset of DMA2 is CCSRBAR + 0x10_1000;

Regards,

Bulat

0 Kudos
Reply