interrupt low time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

interrupt low time

1,184件の閲覧回数
amit123
Contributor I

Hi all,

I want to now what is the minimum low time required for PowerPC  interrupt to detect as a valid interrupt.

Pls guide with proper reference.

0 件の賞賛
返信
1 返信

1,124件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

Typically the minimum low time required for PowerPC interrupt to detect as a valid interrupt provided in the data sheet of particular PowerPC device as AC characteristic of its IRQ input. For example the P2020 data sheet (P2020EC) says “when an external interrupt signal is asserted it must remain the assertion for at least 3 system clocks (SYSCLK periods).”

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信