P3041 DMA Base address.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P3041 DMA Base address.

ソリューションへジャンプ
1,862件の閲覧回数
dshard
Contributor I

Hello!

Can u help me with P3041 DMA base adrress plese?

タグ(1)
0 件の賞賛
返信
1 解決策
1,695件の閲覧回数
Bulat
NXP Employee
NXP Employee

I am not sure what you mean, probably location of the DMA blocks in the internal memory map?

Offset of DMA1  is CCSRBAR + 0x10_0000;

offset of DMA2 is CCSRBAR + 0x10_1000;

Regards,

Bulat

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,696件の閲覧回数
Bulat
NXP Employee
NXP Employee

I am not sure what you mean, probably location of the DMA blocks in the internal memory map?

Offset of DMA1  is CCSRBAR + 0x10_0000;

offset of DMA2 is CCSRBAR + 0x10_1000;

Regards,

Bulat

0 件の賞賛
返信