P2020 RDB PCA, SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P2020 RDB PCA, SDK

3,763件の閲覧回数
hammadnayeem
Contributor II

We ordered 3 P2020RDB-PCA .Out of them one was not working on arrival and other got faulty. We sent both for replacement/repair.

We received Rev D of the boards (referred to as 0.5 in QSG and D1 in schematic) with SDK v1.3 BSP files.
While we had sent Rev E for replacement / repair(referred to as 0.6 in QSG and D2 in schematic).
I have developed my application on SDKv1.7, so I need to run the BSP images of SDKv1.7 on the board we received (Rev. D), but while doing so I am getting error as attached.

The same BSP images of SDKv1.7 are working fine with Rev E of the board we have.

0 件の賞賛
返信
3 返答(返信)

3,563件の閲覧回数
adeel
Contributor III

Hi Hammad,

Are you sure you are using the same ramdisk image on all boards?

BR

Adeel

0 件の賞賛
返信

3,563件の閲覧回数
hammadnayeem
Contributor II

Yes, I am using same image as from SDKv1.7 for all boards. For Rev E its working fine but for Rev D it is showing error as attached previously.

Regards,

Hammad Nayeem

Executive - ICT

Tata Advanced Systems Ltd.

B-11, Sector 4

Noida

0 件の賞賛
返信

3,563件の閲覧回数
adeel
Contributor III

Hi Hammad,

Is your problem solved? If not then you should define the correct flash image type in your DTS file. It looks to me like the Rev.D and Rev.E has different flash memories on the board. So, the same DTS file will not work.

0 件の賞賛
返信