OpenWrt on T1040 processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OpenWrt on T1040 processor

ソリューションへジャンプ
3,927件の閲覧回数
uvmbox
Contributor III

Is it possible to install OpenWrt to t1040 based board? Why LSDK does not have this option?

0 件の賞賛
返信
1 解決策
3,871件の閲覧回数
uvmbox
Contributor III

I added new configuration to openwrt, and was able to compile it for t104x boards!!! Now it works!!! I very satisfied to have luci web interface, package manager and other components easy to install and configure on my device. now I like OpenWrt more than yocto )

uvmbox_0-1608714142630.png

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,872件の閲覧回数
uvmbox
Contributor III

I added new configuration to openwrt, and was able to compile it for t104x boards!!! Now it works!!! I very satisfied to have luci web interface, package manager and other components easy to install and configure on my device. now I like OpenWrt more than yocto )

uvmbox_0-1608714142630.png

 

0 件の賞賛
返信
3,921件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

OpenWrt doens't support T1040, LSDK only support Layerscape platforms, doesn't support T1040 either.

 

You could use Yocto 3.1 release, please refer to

https://source.codeaurora.org/external/qoriq/qoriq-components/yocto-sdk/tree/readme?h=dunfell

0 件の賞賛
返信
3,913件の閲覧回数
uvmbox
Contributor III

there is an openwrt layer for yocto https://github.com/kraj/meta-openwrt .  It has main components of openwrt UCI -command line interface, LUCI web interface and some others. I was able to to compile it for t1040 based board, but to make it work i have to go more deep. The other way is to add new platform support to openwrt SDK. Was someone go these ways and had achived any result? Can be there  something to makes it hard or impossible?

0 件の賞賛
返信