Connection schematics for the second bank is just the same as for the first one, just MCS1, MCKE1 and MODT1 should be used in place of MCS0, MCKE0 and MODT0.
Note that because of fly-by topology SDRAM chips of the second bank have to be placed under the chips of first bank on the opposite board surface (as on DIMM module).
General reference is AN3940 - Hardware and Layout Design Considerations for DDR3 SDRAM.