Multibank DDR3 Interface!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multibank DDR3 Interface!

Jump to solution
1,811 Views
qammarabbas
Contributor IV

Hi,

I am interfacing 2 banks of DDR3L devices with T1042 processor. At this stage, i have got some schematics for reference but all of them either use a single bank or they use registered DIMMS. Can anybody please provide a schematic having multiple banks? I want to see how are the different groups (Address, Command, Control) terminated.

Thank you!

Tags (1)
0 Kudos
Reply
1 Solution
1,637 Views
ufedor
NXP Employee
NXP Employee

Connection schematics for the second bank is just the same as for the first one, just MCS1, MCKE1 and MODT1 should be used in place of MCS0, MCKE0 and MODT0.

Note that because of fly-by topology SDRAM chips of the second bank have to be placed under the chips of first bank on the opposite board surface (as on DIMM module).

General reference is AN3940 - Hardware and Layout Design Considerations for DDR3 SDRAM.

View solution in original post

0 Kudos
Reply
3 Replies
1,638 Views
ufedor
NXP Employee
NXP Employee

Connection schematics for the second bank is just the same as for the first one, just MCS1, MCKE1 and MODT1 should be used in place of MCS0, MCKE0 and MODT0.

Note that because of fly-by topology SDRAM chips of the second bank have to be placed under the chips of first bank on the opposite board surface (as on DIMM module).

General reference is AN3940 - Hardware and Layout Design Considerations for DDR3 SDRAM.

0 Kudos
Reply
1,637 Views
qammarabbas
Contributor IV

Thank you. I want to know about how to terminate the address, clock and command group. Can you please elaborate that?

0 Kudos
Reply
1,637 Views
ufedor
NXP Employee
NXP Employee

In case of two banks all these signals should be terminated the same way as in case of single bank.

0 Kudos
Reply