MPC8347 CPU Local Bus Timing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC8347 CPU Local Bus Timing

1,491 次查看
sharper
Contributor III

With the DLL in bypass mode and with OR[EAD] set to 0, LALE should be asserted for one bus clock cycle only.

What is the hold time of the LALE signal from the falling edge of LCLK?

标记 (2)
0 项奖励
回复
1 回复

1,304 次查看
r8070z
NXP Employee
NXP Employee

Have a great day,

It is not specified as for LALE as for LAD in the DLL bypass mode. Only LAD hold time from the falling edge of LALE is specified in this mode. It is supposed that address is latched on LALE transition while LCLK is irrelevant in this case.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复