MPC8347 CPU Local Bus Timing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC8347 CPU Local Bus Timing

1,460件の閲覧回数
sharper
Contributor III

With the DLL in bypass mode and with OR[EAD] set to 0, LALE should be asserted for one bus clock cycle only.

What is the hold time of the LALE signal from the falling edge of LCLK?

タグ(2)
0 件の賞賛
返信
1 返信

1,273件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

It is not specified as for LALE as for LAD in the DLL bypass mode. Only LAD hold time from the falling edge of LALE is specified in this mode. It is supposed that address is latched on LALE transition while LCLK is irrelevant in this case.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信