Linux driver for eMMC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Linux driver for eMMC

跳至解决方案
6,610 次查看
ihaymov
Contributor II

Hello.

I would like to know if there is a driver for eMMC chip:

MTFC8/16/32/64/128GAP made by Micron (vendor)

The driver is for Linux.

I am targeting to work with LS1046A using the latest Linux Kernel of 4.x.x version (supplied/distributed as yocto) as supported by the NXP staff/community.

If there is no specific driver - what can I do to modify an existent driver of other eMMC memory chip?

Here is a link of the eMMC datasheet:

https://www.micron.com/-/media/client/global/documents/products/data-sheet/emmc/automotive/auto_emmc... 

Thank you.

标记 (3)
0 项奖励
回复
1 解答
5,642 次查看
Pavel
NXP Employee
NXP Employee

NXP Linux BSP for the LS1046a supports eMMC 4.5. See documentation for this BSP.

The MTFC8/16/32/64/128GAP documentation shows that these eMMC are backward compatible with previous MMC. It means that special driver is not needed for this eMMC.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
5,643 次查看
Pavel
NXP Employee
NXP Employee

NXP Linux BSP for the LS1046a supports eMMC 4.5. See documentation for this BSP.

The MTFC8/16/32/64/128GAP documentation shows that these eMMC are backward compatible with previous MMC. It means that special driver is not needed for this eMMC.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------