[LS1046A] Inquiries regarding PCB Layout

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[LS1046A] Inquiries regarding PCB Layout

ソリューションへジャンプ
2,041件の閲覧回数
heesoo_ahn
Contributor I

To whom may it concern.

 

Hello, I'm HS.

 

I wonder if there are application notes or guide for PCB Layout as to LS1046A, LS1046ARDB, or FRWYLS1046

 

All i found was the document regarding DDR4 which is called AN5097 and i want more information.

 

Thank you 

0 件の賞賛
返信
1 解決策
2,037件の閲覧回数
ufedor
NXP Employee
NXP Employee

There is no application note concerning PCB layout for the LS1046A specifically.

 

The following application note will be useful for high-speed serial signals layout:

https://www.nxp.com/webapp/Download?colCode=AN3656&location=null

It is recommended to refer to the general recommendations provided in the processor's Design Checklist:

https://www.nxp.com/docs/en/application-note/AN5252.pdf

Also please consider that NXP evaluation boards have corresponding design data packages containing layout files and it is possible to re-use the PCB layout design constraints from them:

https://www.nxp.com/downloads/en/printed-circuit-boards/LS1043ARDB_PD-39019-DF.zip

https://www.nxp.com/downloads/en/printed-circuit-boards/FRWY-LS1046A-PA-DF.zip

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,038件の閲覧回数
ufedor
NXP Employee
NXP Employee

There is no application note concerning PCB layout for the LS1046A specifically.

 

The following application note will be useful for high-speed serial signals layout:

https://www.nxp.com/webapp/Download?colCode=AN3656&location=null

It is recommended to refer to the general recommendations provided in the processor's Design Checklist:

https://www.nxp.com/docs/en/application-note/AN5252.pdf

Also please consider that NXP evaluation boards have corresponding design data packages containing layout files and it is possible to re-use the PCB layout design constraints from them:

https://www.nxp.com/downloads/en/printed-circuit-boards/LS1043ARDB_PD-39019-DF.zip

https://www.nxp.com/downloads/en/printed-circuit-boards/FRWY-LS1046A-PA-DF.zip

 

0 件の賞賛
返信