LS1012A USB3 peripheral mode performance or benchmark?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1012A USB3 peripheral mode performance or benchmark?

1,326件の閲覧回数
tianfuma
Contributor I

Is there any benchmark data on ls1012a's usb 3 in peripheral mode? such as usb gadget / mass storage or cdc/rndis?

We are looking for a hardware platform which can provide a usb transfer rate well over 50MBytes / sec in peripheral mode, at least when transferring a large file using mtp or usb mass storage driver. Can ls1012a meet such requirement?

タグ(1)
0 件の賞賛
返信
1 返信

1,198件の閲覧回数
andrei_skok
NXP Employee
NXP Employee

As of now we don't have any such numbers.

0 件の賞賛
返信