LS1012A USB3 peripheral mode performance or benchmark?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1012A USB3 peripheral mode performance or benchmark?

1,339 Views
tianfuma
Contributor I

Is there any benchmark data on ls1012a's usb 3 in peripheral mode? such as usb gadget / mass storage or cdc/rndis?

We are looking for a hardware platform which can provide a usb transfer rate well over 50MBytes / sec in peripheral mode, at least when transferring a large file using mtp or usb mass storage driver. Can ls1012a meet such requirement?

Tags (1)
0 Kudos
Reply
1 Reply

1,211 Views
andrei_skok
NXP Employee
NXP Employee

As of now we don't have any such numbers.

0 Kudos
Reply