LS1012A I2S and ESAI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1012A I2S and ESAI

1,297 Views
emagnioj
Contributor II

Is there a datasheet with timing for I2S and ESAI? Does LS1012A I2S support 50Mhz (bitclock)?

Is there a reference manual available?

Thank you!

Dom

0 Kudos
Reply
1 Reply

1,153 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

The LS1012A Datasheet & Reference Manual are labeled as Preliminary Confidential Proprietary - Non-Disclosure Agreement (NDA) required . Please ensure that your company has active signed NDA with NXP/Freescale, if not please use the Phone Support to arrange the NDA signing:  Sales and Support|NXP
To obtain the documents please create a Technical Case: How I could create a Service Request? | NXP Community

As I can see in the datasheet minimal bit clock (SAIn_TX_BCLK/SAIn_RX_BCLK) cycle time is 20 ns.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------