U-boot prompt not coming in T4240 board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

U-boot prompt not coming in T4240 board

1,066 Views
smitagumansingh
Contributor I

Hi ,

Unfortunately my T4240 board got bricked and I am unable to get u-boot prompt. Please help me to unbrick my T4240 board .

0 Kudos
Reply
5 Replies

908 Views
smitagumansingh
Contributor I

Hi Ufedor,

I have installed CodeWarrior on my window machine but unable to perform NOR Flash from the ISO image. Is there any document or QSG to follow flashing of an image using CodeWarrior  USB TAB ?

0 Kudos
Reply

908 Views
ufedor
NXP Employee
NXP Employee

Please refer to the following section in the SDK Documentation:

Submit Form 

0 Kudos
Reply

908 Views
ufedor
NXP Employee
NXP Employee

If the board is T4240RDB you can try to boot from the alternative NOR Flash bank by setting SW3(3:1)=OFF-ON-ON.

0 Kudos
Reply

908 Views
smitagumansingh
Contributor I

Hi Ufedor,

Thanks for the quick reply. I tried by changing SW3 switch setting to SW3(3:1)=OFF-ON-ON , still u-boot prompt is not coming. Any other way to get it back ??

0 Kudos
Reply

908 Views
ufedor
NXP Employee
NXP Employee

In this case it is required to use CodeWarrior Flash Programmer to restore complete NOR Flash from the image provided in the SDK Source ISO availabled at:

https://freescaleesd.flexnetoperations.com/337170/477/10318477/QorIQ%20Linux%20SDK%20v2.0%20PPC64E65... 

0 Kudos
Reply