LS1012A soft reset via memory write

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1012A soft reset via memory write

2,033 Views
nattapongsungch
Contributor III

Hi , 

I tried to do a Soft reset via memory writing from U-boot. 

What i have done on U-boot is.

 

Issue 0x1570204 , Core soft reset enable control register (CORESRENCR)
=> mw 1570204 ffffffff

Issue 0x1570130 , Core0 soft reset register (CORE0_SFT_RST)

=> mw 1570130 ffffffff

Then chip not reset.

I'm not sure it is correct register or soft reset sequence is correct or not. 

Thank you,

Nattapong

1 Reply

1,879 Views
ufedor
NXP Employee
NXP Employee

It is needed to check that the GIC interrupt mapping is performed correctly.

Please refer to the QorIQ LS1012A Reference Manual, 4.4.2 Core Soft Reset.