In LS1043A, Debug Console Port Using UART

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

In LS1043A, Debug Console Port Using UART

1,588 Views
logeshs
Contributor II

Hi,

We have connected UART1 to Data Switch (Trident 2+). Shall we use UART2 as Debug console port in LS1043A? Please confirm.

Thanks

0 Kudos
Reply
2 Replies

1,417 Views
alexander_yakov
NXP Employee
NXP Employee

From the hardware point of view, LS1046A does not need console debug port, debugging is performed via special debigging connector. If you mean console output of particular software, for example U-boot, than this software can be configured as you wish.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,417 Views
logeshs
Contributor II

Thanks for your clarification.

We are just looking for optional console output. 

Thanks.

0 Kudos
Reply