In LS1043A, Debug Console Port Using UART

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

In LS1043A, Debug Console Port Using UART

1,667件の閲覧回数
logeshs
Contributor II

Hi,

We have connected UART1 to Data Switch (Trident 2+). Shall we use UART2 as Debug console port in LS1043A? Please confirm.

Thanks

0 件の賞賛
返信
2 返答(返信)

1,496件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

From the hardware point of view, LS1046A does not need console debug port, debugging is performed via special debigging connector. If you mean console output of particular software, for example U-boot, than this software can be configured as you wish.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,496件の閲覧回数
logeshs
Contributor II

Thanks for your clarification.

We are just looking for optional console output. 

Thanks.

0 件の賞賛
返信