Hi !

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决
1,998 次查看
muhammadmoosa
Contributor I

I am working with T1042. I want to interface this processor with xilinx spartan 6 FPGA. What is the best possible option?

0 项奖励
回复
1 解答
1,942 次查看
alexander_yakov
NXP Employee
NXP Employee

Typical most commonly used connection type for FPGA is parallel connection to IFC controller.

In addition, Spartan 6 has a number of high-speed interface blocks, for example - PCI-Express.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
1,943 次查看
alexander_yakov
NXP Employee
NXP Employee

Typical most commonly used connection type for FPGA is parallel connection to IFC controller.

In addition, Spartan 6 has a number of high-speed interface blocks, for example - PCI-Express.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,942 次查看
muhammadmoosa
Contributor I

Thanks 

0 项奖励
回复