Hi !

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
1,959 Views
muhammadmoosa
Contributor I

I am working with T1042. I want to interface this processor with xilinx spartan 6 FPGA. What is the best possible option?

0 Kudos
Reply
1 Solution
1,903 Views
alexander_yakov
NXP Employee
NXP Employee

Typical most commonly used connection type for FPGA is parallel connection to IFC controller.

In addition, Spartan 6 has a number of high-speed interface blocks, for example - PCI-Express.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
1,904 Views
alexander_yakov
NXP Employee
NXP Employee

Typical most commonly used connection type for FPGA is parallel connection to IFC controller.

In addition, Spartan 6 has a number of high-speed interface blocks, for example - PCI-Express.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,903 Views
muhammadmoosa
Contributor I

Thanks 

0 Kudos
Reply