Hi !

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,964件の閲覧回数
muhammadmoosa
Contributor I

I am working with T1042. I want to interface this processor with xilinx spartan 6 FPGA. What is the best possible option?

0 件の賞賛
返信
1 解決策
1,908件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Typical most commonly used connection type for FPGA is parallel connection to IFC controller.

In addition, Spartan 6 has a number of high-speed interface blocks, for example - PCI-Express.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,909件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Typical most commonly used connection type for FPGA is parallel connection to IFC controller.

In addition, Spartan 6 has a number of high-speed interface blocks, for example - PCI-Express.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,908件の閲覧回数
muhammadmoosa
Contributor I

Thanks 

0 件の賞賛
返信