Create SD Card Image for LS1043ARDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Create SD Card Image for LS1043ARDB

ソリューションへジャンプ
2,086件の閲覧回数
aismail102
Contributor II

Question 

How do I generate an SD card image in Yocto for the LS1043ARDB? I've read about the WIC tool and I see some wks files for the IMX processors, however, I don't see any for the layerscape parts. My issue is that the QorIQ memory layout doesn't seem compatible with WIC ( I could be mistaken). Options like --offset and --align are in (Kbyte boundaries), but the RCW+PBL+BL2 starts at 0x8. Is the WIC tool the right way to go?

 

Current Status

I have an image that works with a Yocto generated bootloader, dt, kernel, and file system. I want Yocto to create an sdcard image that will place them in the proper places in memory.

0 件の賞賛
返信
1 解決策
2,077件の閲覧回数
aismail102
Contributor II

Problem solved, on reading the guide closer the memory layout for the SD card is described in block numbers and not a physical address. 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,078件の閲覧回数
aismail102
Contributor II

Problem solved, on reading the guide closer the memory layout for the SD card is described in block numbers and not a physical address. 

0 件の賞賛
返信