Create SD Card Image for LS1043ARDB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Create SD Card Image for LS1043ARDB

跳至解决方案
2,090 次查看
aismail102
Contributor II

Question 

How do I generate an SD card image in Yocto for the LS1043ARDB? I've read about the WIC tool and I see some wks files for the IMX processors, however, I don't see any for the layerscape parts. My issue is that the QorIQ memory layout doesn't seem compatible with WIC ( I could be mistaken). Options like --offset and --align are in (Kbyte boundaries), but the RCW+PBL+BL2 starts at 0x8. Is the WIC tool the right way to go?

 

Current Status

I have an image that works with a Yocto generated bootloader, dt, kernel, and file system. I want Yocto to create an sdcard image that will place them in the proper places in memory.

0 项奖励
回复
1 解答
2,081 次查看
aismail102
Contributor II

Problem solved, on reading the guide closer the memory layout for the SD card is described in block numbers and not a physical address. 

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,082 次查看
aismail102
Contributor II

Problem solved, on reading the guide closer the memory layout for the SD card is described in block numbers and not a physical address. 

0 项奖励
回复