Create SD Card Image for LS1043ARDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Create SD Card Image for LS1043ARDB

Jump to solution
2,067 Views
aismail102
Contributor II

Question 

How do I generate an SD card image in Yocto for the LS1043ARDB? I've read about the WIC tool and I see some wks files for the IMX processors, however, I don't see any for the layerscape parts. My issue is that the QorIQ memory layout doesn't seem compatible with WIC ( I could be mistaken). Options like --offset and --align are in (Kbyte boundaries), but the RCW+PBL+BL2 starts at 0x8. Is the WIC tool the right way to go?

 

Current Status

I have an image that works with a Yocto generated bootloader, dt, kernel, and file system. I want Yocto to create an sdcard image that will place them in the proper places in memory.

0 Kudos
Reply
1 Solution
2,058 Views
aismail102
Contributor II

Problem solved, on reading the guide closer the memory layout for the SD card is described in block numbers and not a physical address. 

View solution in original post

0 Kudos
Reply
1 Reply
2,059 Views
aismail102
Contributor II

Problem solved, on reading the guide closer the memory layout for the SD card is described in block numbers and not a physical address. 

0 Kudos
Reply