Debug U-boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debug U-boot

2,035件の閲覧回数
canvanquyen
Contributor III

Hi everybody,

Currently, I'm working in B4860QDS development board.

I try to debug u-boot in this board but I have some problem bellow.

I read doc(AN4876.pdf) It guides to debug u-boot. I shows we need B4860QDS_uboot_32.tcl initialization file for B4860 chipset.

But in "C:\Freescale\CW_PA_v10.5.0\PA\PA_Support\Initialization_Files\Qonverge" directory does not have this file.

Can you tell me how i can get this file to debug u-boot on this chipset?

Thanks & best regards,

Quyen.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,865件の閲覧回数
addiyi
NXP Employee
NXP Employee

Hi Quyen,

After attach to u-boot, when uboot.tcl file is not available, you can reset the board from reset button with no initialization file.

Adrian

0 件の賞賛
返信