Dear all,
As I know, Booting from SPI flash. First of all, device will sample cfg_rcw_src[0:8]( SW1.0:7 & SW2.1) to determine where it starts to get RCW & PBI cmd.
If cfg_rcw_src[0:8] selected for SPI FLASH, B4860 will load RCW to RCWSRn , PBI to CCSR, SPL to SDRAM.
As I know :
In PBI cmd that enable SPI interface ("board/freescale/b4860qds/b4_pbi.cfg").
#Configure SPI controller
09110000 80000403
09110020 2d170008
09110024 00100008
09110028 00100008
0911002c 00100008
My question is :
How B4860 can load RCW, PBI to RCWSR and CCSR memory if SPI controller did not enable?
Could someone help me understand this process in B4860.
Thank you very much!
已解决! 转到解答。
Hi Can
PBL (Pre-boot Loader) initializes the controller. The
chapter "Pre-Boot Loader (PBL)" in your B4860 Reference
Manual explains more in detail which peripherals it initializes
to load RCW and boot from. Please refer to that chapter
for more detailed information.
Regards
Sinan Akman
Hi Can
PBL (Pre-boot Loader) initializes the controller. The
chapter "Pre-Boot Loader (PBL)" in your B4860 Reference
Manual explains more in detail which peripherals it initializes
to load RCW and boot from. Please refer to that chapter
for more detailed information.
Regards
Sinan Akman
Hi, Sinan Akman,
Thanks for your answer.
I found that in the reference.
5.3 PBL Modes of Operation
• Load both RCW and pre-boot initialization commands from individual interface.
• Load RCW only.
• Load pre-boot initialization commands only if default RCW is to be used.
So that we need to re-initialize SPI again in PBI command.
Is that correct?
Thanks.
Hi Can
You don't need to re-initialize SPI, but as listed on
your PBI :
09110020 2d170008
09110024 00100008
09110028 00100008
0911002c 00100008
It sets the mod register for
the underlying hardware.
PBL initializes SPI controller so
that it can access it for RCW, PBI etc.
Then if there is PBI, it executes
it to set/modify registers for the platform
design.
Regards
Sinan Akman